Other Parts Discussed in Thread: AMIC110
I would like to get the DCAN Example Running on an AMIC110_ICE_EVM Board.
I connected a CAN Interface Chip: https://www.nxp.com/docs/en/data-sheet/PCA82C250.pdf
To D17 and D18. Acording to the Datasheet of the AM335X Family this should allow me to use the DCAN0 Interface.
Then i build the pdk starterware examples (E:\ti\pdk_am335x_1_0_17\packages\ti\starterware\examples)
and Deployed the dcan frame_tx_rx example (E:\ti\pdk_am335x_1_0_17\packages\ti\starterware\examples\dcan\frame_tx_rx)
BOARDInit status [0x0]
SoC : [AM335X]
Core : [A8]
Board Detected : [AMIC110]
Base Board Revision : [UNKNOWN]
Daughter Card Revision: [UNKNOWN]
Invalid device ID!!
Device is not available on this board!
FAILURE!!!
I am now looking through the Code but i havent found the Code where i can tell that the Board has a CAN Controller and how it should Configure the PinMux.