Texas Instruments (TI) Processors support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search processors content or ask technical support questions on Sitara™ processors, digital signal processors (DSP) and automotive processors. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
Part Number: PROCESSOR-SDK-DRA8X-TDA4X I see there is only one target option for assigning a given OpenVX node to one of J7’s heterogeneous cores. If I have multiple nodes that need to run on one of these cores, how is this treated by the framework? Do…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X I have two algorithms that I would like to use on a given core within J7. Should I wrap these algorithms into two different OpenVX nodes within my OpenVX graph or should they be a single node?
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
Hi Ti,
From the developer notes for release PROCESSOR-SDK-LINUX-DRA8X-TDA4X : V06.02.00.07 i can see instructions for using rootfs from emmc.
For booting we still need uboot from the connected SDCARD. I copied…
Part Number: TDA4VM I have a remote core firmware that is printing debug traces, and I have QNX HLOS running on A72. How can I view the remote core traces with QNX HLOS?
I'm using SYS/BIOS (the TI-RTOS kernel) in an application. I call System_printf, but I'm not sure where the output is going to. It is not being shown in the console. Help!
Part Number: PROCESSOR-SDK-DRA8X-TDA4X Other Parts Discussed in Thread: DRA829 , TDA4VM
I would like to integrate Jacinto 7 safety features into my software. How do I get started adding safety features to my software?
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
I get the following error messages during vxVerifyGraph in OpenVX. How do I fix this issue?
VX_ZONE_ERROR:[ownContextSendCmd:553] Command ack message returned failure cmd_status: -1
VX_ZONE_ERROR:[ownNodeKernelInit…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
When I try to create a new node in OpenVX, I get the following error message on the target CPU:
"tivxTargetKernelInstanceAlloc: kernel <kernel name> has not been registered on this CPU"
I also get the following…