Hello,
I would like to ask if it is possible to work with only one bank of DDR , how to disable one of the banks (for power save) with DM814x
Thank you,
Ran
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Pavel,
I've tried to patch my source files according to the FAQ and patch you've provided, but the board fails to start.
It seems that the error is related to the LISA configuration ,
These are the lisa registers I'm using for 256M (singl EMIF) configuration.
/* SINGLE EMIF LISA MAP */
#define MIN_DMM_LISA_MAP__3 0x80500100
....
#ifdef DDR_MEM_512M
__raw_writel(0x80540300, DMM_LISA_MAP__0);
__raw_writel(0xA0540300, DMM_LISA_MAP__1);
__raw_writel(0x80540300, DMM_LISA_MAP__2);
if(USE_EMIF1) {
__raw_writel(0xA0540300, DMM_LISA_MAP__3);
} else {
__raw_writel(MIN_DMM_LISA_MAP__3, DMM_LISA_MAP__3);
}
while (__raw_readl(DMM_LISA_MAP__0) != 0x80540300);
while (__raw_readl(DMM_LISA_MAP__1) != 0xA0540300);
while (__raw_readl(DMM_LISA_MAP__2) != 0x80540300);
while (__raw_readl(DMM_LISA_MAP__3) != 0xA0540300);
#else
.....
I think that the original patch is relevant for 1G only (
#define PG2_1_DMM_LISA_MAP__0 0x0
#define PG2_1_DMM_LISA_MAP__1 0x0
#define PG2_1_DMM_LISA_MAP__2 0x0
#define PG2_1_DMM_LISA_MAP__3 0x80640300
)
Do you have any idea ?
Regards,
Ran
Ran,
Could you try with revert back this patch and apply the below modifications instead of this patch
u-boot/arch/arm/include/asm/arch-ti81xx/ddr_defs_ti814x.h
#define PG2_1_DMM_LISA_MAP__0 0x0
#define PG2_1_DMM_LISA_MAP__1 0x0
#define PG2_1_DMM_LISA_MAP__2 0x0
#define PG2_1_DMM_LISA_MAP__3 0x80400100 0x80640300
u-boot/board/ti/ti8148/evm.c
static void config_ti814x_ddr(void)
{
__raw_writel(0x2, CM_DEFAULT_EMIF_0_CLKCTRL); /*Enable EMIF0 Clock*/
__raw_writel(0x2, CM_DEFAULT_EMIF_1_CLKCTRL); /*Enable EMIF1 Clock*/
/*Poll for Module is functional*/
while ((__raw_readl(CM_DEFAULT_EMIF_0_CLKCTRL)) != 0x2);
while ((__raw_readl(CM_DEFAULT_EMIF_1_CLKCTRL)) != 0x2);
Hi Pavel,
The original configuration I'm using (512M) is as following:
__raw_writel(0x80540300, DMM_LISA_MAP__0);
__raw_writel(0xA0540300, DMM_LISA_MAP__1);
__raw_writel(0x80540300, DMM_LISA_MAP__2);
__raw_writel(0xA0540300, DMM_LISA_MAP__3);
When configuring it as following (without any other modifications in code), it fails:
__raw_writel(0, DMM_LISA_MAP__0);
__raw_writel(0, DMM_LISA_MAP__1);
__raw_writel(0, DMM_LISA_MAP__2);
__raw_writel(0x80500100 , DMM_LISA_MAP__3);
I will now try to add the modification you've described in config_ti814x_ddr(), and see if it makes any differences:
static void config_ti814x_ddr(void)
{
__raw_writel(0x2, CM_DEFAULT_EMIF_0_CLKCTRL); /*Enable EMIF0 Clock*/
__raw_writel(0x2, CM_DEFAULT_EMIF_1_CLKCTRL); /*Enable EMIF1 Clock*/
/*Poll for Module is functional*/
while ((__raw_readl(CM_DEFAULT_EMIF_0_CLKCTRL)) != 0x2);
while ((__raw_readl(CM_DEFAULT_EMIF_1_CLKCTRL)) != 0x2);
...
Thank you very much for the assistance !!
Ran
Ran,
Ran Shalit said:though the u-boot printing still shows me 512M instead of 256M ..........
This print is just for info. The default print is for 2GB DDR (by mistake) and fixed to 1GB with the below patch:
Have you tried with modifying ti8148_evm.h like below? This is for single EMIF, 256MB DDR3
#define CONFIG_NR_DRAM_BANKS 1 /* we have 1 bank of DRAM */
#define PHYS_DRAM_1 0x80000000 /* DRAM Bank #1 */
#define PHYS_DRAM_1_SIZE 0x10000000 /* 256 MB */
U-Boot 2010.06-dirty (Mar 24 2015 - 10:56:21) TI8148-GP rev 3.0 L3 clk : 200MHz IVA clk : 410MHz ISS clk : 480MHz DSP clk : 750MHz DSS clk : 200MHz ARM clk : 720MHz DDR clk : 400MHz DRAM: 512 MiB NAND: HW ECC BCH8 Selected 512 MiB Using default environment The 2nd stage U-Boot will now be auto-loaded Hit any key to stop autoboot: 0 NAND read: device 0 offset 0x20000, size 0x40000 262144 bytes read: OK ## Starting application at 0x81000000 ... U-Boot 2010.06-dirty (Oct 30 2014 - 09:56:38) TI8148-GP rev 3.0 L3 clk : 200MHz IVA clk : 410MHz ISS clk : 480MHz DSP clk : 750MHz DSS clk : 200MHz ARM clk : 720MHz DDR clk : 400MHz ------------ PLL Settings -------------- OSC_0_FREQ : 20MHz MODENA_N : 1 MODENA_M : 72 MODENA_M2 : 1 L3_N : 19 L3_M : 800 L3_M2 : 4 DSP_N : 19 DSP_M : 750 DSP_M2 : 1 DSS_N : 19 DSS_M : 800 DSS_M2 : 4 IVA_N : 19 IVA_M : 820 IVA_M2 : 2 ISS_N : 19 ISS_M : 960 ISS_M2 : 2 USB_N : 19 USB_M : 960 USB_M2 : 5 DCO_HS2_MIN : 500 DCO_HS2_MAX : 1000 DCO_HS1_MIN : 1000 DCO_HS1_MAX : 2000 SELFREQDCO_HS2 : 2049 SELFREQDCO_HS1 : 4097 --------- DDR PLL ---------- DDR_N : 0x13 DDR_M : 0x320 DDR_M2 : 0x2 ----------EMIF Timings (identical for 0 & 1)------- DDR3_EMIF_READ_LATENCY : 0x170209 DDR3_EMIF_TIM1 : 0xAAAD4E3 DDR3_EMIF_TIM2 : 0x40437FDC DDR3_EMIF_TIM3 : 0x50BF83FF DDR3_EMIF_REF_CTRL : 0xC30 DDR3_EMIF_SDRAM_CONFIG : 0x61C051B2 DDR3_EMIF_SDRAM_ZQCR : 0x50074BE1 ----------ranran disbaled the next prints ----------ranran disbaled the next prints I2C: ready DRAM: 512 MiB NAND: HW ECC BCH8 Selected 512 MiB MMC: OMAP SD/MMC: 0 .:;rrr;;. ,5#@@@@#####@@@@@@#2, ,A@@@hi;;;r5;;;;r;rrSG@@@A, r@@#i;:;s222hG;rrsrrrrrr;ri#@@r :@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@: B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B @@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@ @@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@ @@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@ G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G @9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@ X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X @#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@ @A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@ @&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@ @#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@ M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@# :@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@, @@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@ @A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@ ;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@; r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r ,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@, B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H .@@@i;;ranran MP;rrrrr;r@M:;i@@@. .A@@#5r;;;r;;;rrr;r:r#AsM@@H. ;&@@@@MhXS5i5SX9B@@@@G; :ihM#@@@@@##hs, Net: Detected MACID:7c:66:9d:35:99:6 cpsw Hit any key to stop autoboot: 0 HW ECC BCH8 Selected NAND read: device 0 offset 0x580000, size 0x300000 3145728 bytes read: OK ## Booting kernel from Legacy Image at 81000000 ... Image Name: Linux-2.6.37 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2610568 Bytes = 2.5 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Linux version 2.6.37 (ubuntu@ubuntu-laptop) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #38 Mon Mar 9 16:55:44 IST 2015 CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine: ti8148evm bootconsole [earlycon0] enabled vram size = 52428800 at 0x0 ti81xx_reserve: ### Reserved DDR region @87f00000 reserved size = 52428800 at 0x0 FB: Reserving 52428800 bytes SDRAM for VRAM Memory policy: ECC disabled, Data cache writeback OMAP chip is TI8148 3.0 SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000 after smp_prepare_boot_cpu Built 1 zonelists in Zone order, mobility grouping on. Total pages: 19456 Kernel command line: console=ttyO0,115200n8 ip=10.0.0.2 rw rootdelay=5 ubi.mtd=6,2048 rootfstype=ubifs root=ubi0:rootfs init=/init earlyprintk notifyk.vpssm3_sva=0xBFD00000 mem=128M ddr_mem=512M vram=50M PID hash table entries: 512 (order: -1, 2048 bytes) Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) Memory: 76MB 1MB = 77MB total Memory: 72080k/72080k available, 58992k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xffc00000 - 0xffe00000 ( 2 MB) vmalloc : 0xc8800000 - 0xf8000000 ( 760 MB) lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) modules : 0xbf000000 - 0xbfe00000 ( 14 MB) .init : 0xc0008000 - 0xc0035000 ( 180 kB) .text : 0xc0035000 - 0xc04eb000 (4824 kB) .data : 0xc04ec000 - 0xc053ae40 ( 316 kB) SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 NR_IRQS:407 IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts Total of 128 interrupts on 1 active controller GPMC revision 6.0 Trying to install interrupt handler for IRQ400 Trying to install interrupt handler for IRQ401 Trying to install interrupt handler for IRQ402 Trying to install interrupt handler for IRQ403 Trying to install interrupt handler for IRQ404 Trying to install interrupt handler for IRQ405 Trying to install interrupt handler for IRQ406 Trying to install type control for IRQ407 Trying to set irq flags for IRQ407 OMAP clockevent source: GPTIMER1 at 20000000 Hz Console: colour dummy device 80x30 Calibrating delay loop... 719.25 BogoMIPS (lpj=3596288) pid_max: default: 32768 minimum: 301 Security Framework initialized Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok devtmpfs: initialized TI81XX: Map 0x87f00000 to 0xfe500000 for dram barrier TI81XX: Map 0x40300000 to 0xfe600000 for sram barrier omap_voltage_early_init: voltage driver support not added regulator: core version 0.5 regulator: dummy: NET: Registered protocol family 16 omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting! omap_voltage_add_dev: VDD specified does not exist! OMAP GPIO hardware version 0.1 OMAP GPIO hardware version 0.1 OMAP GPIO hardware version 0.1 OMAP GPIO hardware version 0.1 ranran skip omap2_nand_gpmc_retime ti8148_spi_init [ranran] NOR: Can't request GPMC CS after board_nor_init after phy_register_fixup_for_uid after ti814x_pcf8575_cir_init ranran skip ti814x_pcie_pllcfg ranran remove phy_id update from kernel! ranran skip ti81xx_init_pcie clk get on i2c3 fck failed !!!ti814x_enable_i2c1 clk get on i2c2 fck failed Cannot clk_get ck_32 Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now registered ti81xx_vpss device registered ti81xx_vidout device registered ti81xx on-chip HDMI device registered ti81xx_fb device registered ti81xx_vin device NSS Crypto DMA hardware revision 1.9 @ IRQ 116 bio: create slab <bio-0> at 0 vgaarb: loaded SCSI subsystem initialized USBSS revision 4ea2080b registerd cppi-dma Intr @ IRQ 17 Cppi41 Init Done omap_i2c omap_i2c.1: bus 1 rev4.0 at 400 kHz I2C: Read failed at pcf8575_cir_enable 263 with error code: -121 I2C: Transfer failed at pcf8575_cir_enable 270 with error code: -121 pcf857x: probe of 1-0021 failed with error -121 regulator: VRTC: 1800 mV regulator: VIO: 1500 mV regulator: VDD1: 600 <--> 1500 mV at 1200 mV regulator: VDD2: 600 <--> 1500 mV at 1200 mV regulator: VDDCTRL: 600 <--> 1400 mV at 1200 mV regulator: LDO1: 1100 <--> 3300 mV at 1800 mV regulator: LDO2: 1100 <--> 3300 mV at 1800 mV regulator: LDO3: 1100 <--> 3300 mV at 3300 mV regulator: LDO4: 1100 <--> 3300 mV at 1800 mV regulator: LDO5: 1100 <--> 3300 mV at 3300 mV regulator: LDO6: 1100 <--> 3300 mV at 3300 mV regulator: LDO7: 1100 <--> 3300 mV at 3300 mV regulator: LDO8: 1100 <--> 3300 mV at 1800 mV tps65910 1-002d: No interrupt support, no core IRQ omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz omap_i2c omap_i2c.4: bus 4 rev4.0 at 400 kHz Advanced Linux Sound Architecture Driver Version 1.0.23. Switching to clocksource gp timer musb-hdrc: version 6.0, peripheral, debug=0 musb-hdrc musb-hdrc.0: dma type: dma-cppi41 MUSB controller-0 revision 4ea20800 usb2phy: computed values rxcalib(15)DACs(25 15 15) usb2phy: override computed values rxcalib(15)DACs(25 15 15) usb2phy_config: musb(0) rxcalib done, rxcalib read value 6f6cdf7e musb-hdrc musb-hdrc.0: USB Peripheral mode controller at c881e000 using DMA, IRQ 18 NET: Registered protocol family 2 IP route cache hash table entries: 1024 (order: 0, 4096 bytes) TCP established hash table entries: 4096 (order: 3, 32768 bytes) TCP bind hash table entries: 4096 (order: 2, 16384 bytes) TCP: Hash tables configured (established 4096 bind 4096) TCP reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. NetWinder Floating Point Emulator V0.97 (double precision) PMU: registered new PMU device of type 0 omap-iommu omap-iommu.0: ducati registered omap-iommu omap-iommu.1: sys registered JFFS2 version 2.2. (NAND) � 2001-2006 Red Hat, Inc. msgmni has been set to 140 alg: No test for stdrng (krng) io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) nss_rng nss_rng: NSS Random Number Generator ver. 2.0 Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0 console [ttyO0] enabled, bootconsole disabled console [ttyO0] enabled, bootconsole disabled omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 brd: module loaded loop: module loaded at24 1-0050: 65536 byte 24c512 EEPROM (writable) ahci probe: devid name is ahci ahci CAP register dump =0x6726ff80 Modified ahci CAP register dump =0x6f26ff80 ahci ahci.0: forcing PORTS_IMPL to 0x1 ahci: SSS flag set, parallel bus scan disabled ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst scsi0 : ahci_platform ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16 m25p80 spi1.0: mb85rs2mt (256 Kbytes) Creating 1 MTD partitions on "spi_flash": 0x000000000000-0x000000040000 : "FRAM One Partition" omap2-nand driver initializing ONFI param page 0 valid ONFI flash detected NAND device: Maf ID: 0x2c, Chip ID: 0xac (Micron, NAND 512MiB 1,8V 8-bit) erasesize: 0x20000, writesize: 2048, oobsize: 64 omap2-nand: detected x8 NAND flash Creating 7 MTD partitions on "omap2-nand.0": 0x000000000000-0x000000020000 : "U-Boot-min" 0x000000020000-0x000000260000 : "U-Boot" 0x000000260000-0x000000280000 : "U-Boot Env" 0x000000280000-0x000000580000 : "U-Boot Logo" 0x000000580000-0x0000009c0000 : "Kernel" 0x0000009c0000-0x00000d1e0000 : "File System" 0x00000d1e0000-0x000020000000 : "Reserved" UBI: attaching mtd6 to ubi0 UBI: physical eraseblock size: 131072 bytes (128 KiB) UBI: logical eraseblock size: 126976 bytes UBI: smallest flash I/O unit: 2048 UBI: sub-page size: 512 UBI: VID header offset: 2048 (aligned 2048) UBI: data offset: 4096 ata1: SATA link down (SStatus 0 SControl 300) UBI: max. sequence number: 519 UBI warning: print_rsvd_warning: cannot reserve enough PEBs for bad PEB handling, reserved 11, need 16 UBI: attached mtd6 to ubi0 UBI: MTD device name: "File System" UBI: MTD device size: 200 MiB UBI: number of good PEBs: 1601 UBI: number of bad PEBs: 0 UBI: number of corrupted PEBs: 0 UBI: max. allowed volumes: 128 UBI: wear-leveling threshold: 4096 UBI: number of internal volumes: 1 UBI: number of user volumes: 1 UBI: available PEBs: 0 UBI: total number of reserved PEBs: 1601 UBI: number of PEBs reserved for bad PEB handling: 11 UBI: max/mean erase counter: 3/1 UBI: image sequence number: 806041126 UBI: background thread "ubi_bgt0d" started, PID 48 davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 davinci_mdio davinci_mdio.0: detected phy mask fffffffe davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown CAN device driver interface CAN bus driver for Bosch D_CAN controller 1.0 d_can d_can: d_can device registered (irq=52, irq_obj=53) mice: PS/2 mouse device common for all mice qt602240_ts 1-004a: __qt602240_read_reg: i2c transfer failed qt602240_ts: probe of 1-004a failed with error -5 omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 rtc-rv3049 spi2.1: rtc core: registered rv3049 as rtc1 i2c /dev entries driver Linux video capture interface: v2.00 OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec nss_aes_mod_init: loading NSS AES driver nss-aes nss-aes: NSS AES hw accel rev: 3.2 (context 0 @0x41140000) nss-aes nss-aes: NSS AES hw accel rev: 3.2 (context 1 @0x41141000) nss-aes nss-aes: NSS AES hw accel rev: 3.2 (context 2 @0x411a0000) nss-aes nss-aes: NSS AES hw accel rev: 3.2 (context 3 @0x411a1000) nss_aes_probe: probe() done nss_des_mod_init: loading NSS DES driver nss-des nss-des: NSS DES hw accel rev: 2.2 (context 0 @0x41160000) nss-des nss-des: NSS DES hw accel rev: 2.2 (context 1 @0x41161000) nss_des_probe: probe() done nss_sham_mod_init: loading NSS SHA/MD5 driver nss-sham nss-sham: NSS SHA/MD5 hw accel rev: 4.03 (context 0 @0x41100000) nss-sham nss-sham: NSS SHA/MD5 hw accel rev: 4.03 (context 1 @0x41101000) nss-sham nss-sham: NSS SHA/MD5 hw accel rev: 4.03 (context 2 @0x411c0000) nss-sham nss-sham: NSS SHA/MD5 hw accel rev: 4.03 (context 3 @0x411c1000) nss_sham_probe: probe() done
Hi Pavel,
The Linux get freeze when continuing with kernel boot.
Are there any changes required in kernel too ?
Regards,
Ran
Ran,
You can start with adjusting the bootargs for 256MB memory. Try with ddr_mem=256M (not ddr_mem=512M). In EZSDK 256MB map, mem=145M, and MC_HDVPSS_DESC (HDVPSS_DESC) is at 0xAFD00000 (not 0xBFD00000), may be the same is valid here.
Check also DMM_LISA_MAP registers and CM_DEFAULT_EMIF_1_CLKCTRL/CM_DEFAULT_EMIF_1_CLKCTRL registers settings in linux kernel, and align with the u-boot settings.
BR
Pavel
Hi Pavel,
If I may ask one more about it. We intend to move to 256M.
I think it will also require changed in bld file.
I also see that in memory map AN for the SDK It shows as if DM814x supports only 512M ?
TI8168
• Supports 1GB, 2GB builds
• Linux memory allocated can be 256M or 128M or 512MB for 2GB build
• TI814X
• Supports 512MB build
• Linux memory allocated can be 128M
• TI810X
• Supports 256MB, 512MB builds. Default is 256MB
• Linux memory allocated can be 192/128M for 512MB build & 64M for 256MB build
Thanks,
Ran