Hi,
I am using AM335x processor for our project. My main application is to use the both ethernet outputs of processor in same subnet and different subnet.
Setup: Both ethernet address in same subnet
During testing it is observed that when my both ethernet ip address (i.e. eth0=192.168.100.122 and eth1=192.168.100.116) are in same subnet and connected in ethernet switch, both eth ip are pinging.
Case1: when i remove eth0 cable from switch but eth1 cable is inserted , both the ethernet ip addresses stop pinging.
Case 2: When i remove eth1 cable cable from switch and eth0 cable is already inserted, then also both the ip address are pinging in LAN.
Setup: Both ethernet address in different subnet
During testing it is observed that when my both ethernet ip address (i.e. eth0=192.168.100.122 and eth1=192.168.2.116) are in different subnet and connected in ethernet switch, both eth ip are pinging.
Case1: when i remove eth0 cable from switch but eth1 cable is inserted , both the ethernet ip addresses stop pinging. Ideally, only eth0 should stop pinging insteed of both stopping.
Case 2: When i remove eth1 cable cable from switch and eth0 cable is already inserted, eth0 is pinging and eth1 is stopped which is proper.
So, from above both conditions, it is found that both the ethernet outputs are not working independently as it seems that both ethernet depends on eth0 connection in LAN.
Please guide me the cause of problem and its solution.