Hi,
I have verify that the uart boot is successful on the evm board. (dra742)
but I failed when I tried to verify uart boot on our previous generation product. (dra744)
1st stage boot to MLO is working and the command line shows "u-boot-spl.bin file download completed.
then I try to transmit u-boot.img to DUT through YMODEM, but it's can't working. XMODEM also.
Are there any hardware settings that need to be changed?
thanks for your help