This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X: Configuring USB to full speed



Hi All,

I am currently working with Beaglebone black rev3.

I was evaluating USB RNDIS speed and performance, I have used Debian 8.7 2017-03-19 4GB SD. image to flash SD card.

I understand that USB RNDIS support is provided default. But i need to evaluate the speed with the following configuration:

USB speed : Full speed(12Mbps).

CPU Clock: 600MHz.

I have configured the CPU-clock but i am wondering, how we can configure USB Full-speed because when i do a lsusb -t command it returns the speed for which it is configured i.e high speed.

Do I need to configure in the Kernel and load the module,if so could you please suggest some links where it may have described the steps

Could anyone please help on this?

Thanks in advance.

Best Regards,

Manjunath