Hello,
I ran some CPU bound benchmarks and found that the CPU power consumption is almost negligible when compared to the platform power consumption (even when no peripherals are attached). The CPU power consumption is few 10's of milli watts. Whereas, the platform power consumption is in between (5 to 7 watts). Can anybody comment on this? Especially it looks like platform power is less bound to CPU computation, as it continues to draw the baseline power even after program termination. Is it platform dependent? If yes how?
Also, is there a way to completely power off the USB's, HDMI and other devices on the platform? I have read that at least for the USB's, at the most they can go into suspend mode and it is not possible to completely power them off. I am not exactly sure though.
Thank you for your time.