Part Number: TMDXEVM388
Tool/software: Linux
HI,
I am using TMS320DM38x Evaluation Module and i am using ipnc_rdk3.9.1. I want to configure USB as both ACM and mass storage. So I have selected CDC Composite device(ACM and mass storage ) in menuconfig and also I tried Multi function composite gadget (CDC Ethernet + CDC Serial +Storage configuration) .In both cases the board is not detecting serial and mass storage gadget. Then I have tried in
" M " mode. After compilation the .ko files generated . but I can't insert it (its give "insmod error could not insert module :no such device").
but works fine when I configure USB as serial gadget or mass storage separately.
can anyone tell me what should i do for configure USB as both ACM and mass storage in this board? and mention if i did anything wrong.
Thanks in advance