Part Number: AM3358
Hello!
I mentioned some strange behavior, while playing with baremetal CPSW ethernet driver on beagle bone black.
The described scenario reproduces with ping flood & small packet size, which gives huge amount of CPSW interrupts
Actually, the pattern looks like:
1. Some code sets INTC_IRQ_THRESHOLD in omap intc to 24
2. CPSW RX interrupt is arriving (irq # 41)
3. In CPSW irq handler I dump interrupt controller registers and see the following:
INTC_SIR_IRQ: 0x29
INTC_IRQ_PRIORITY: 0x2c
INTC_IRQ_THRESHOLD: 0x18
INTC_ILR 40: 0x0
INTC_ILR 41: 0xb0
INTC_ILR 42: 0xb0
INTC_ILR 43: 0x0
Which means irq 41 has arrived (0x29) it has priority 44 (0x2c) while priority
threshold is 24 (0x18). According reference manual 6.1.1.4 0x0 is the highest priority,
while 0x7F is the lowest. If so i can't clearly understand: how could we get
IRQ with priority 44, while threshold is was set to 24? Any suggestions about that?
Am i miss something?
Thank you.