Other Parts Discussed in Thread: PMP, BEAGLEBOARD-X15, , DRA752
Tool/software: Linux
Hi all,our custom board boot from sd card failed ,the log ouput as follow:
U-Boot SPL 2016.05 (Dec 16 2017 - 21:23:37)
DRA752-GP ES2.0
Trying to boot from MMC1
i2c_write: error waiting for addr ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
U-Boot 2016.05 (Dec 16 2017 - 21:23:37 +0800)
CPU : DRA752-GP ES2.0
Board: UNKNOWN(BeagleBoard X15?) REV UNKNOWN
I2C: ready
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
i2c_write: error waiting for addr ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
i2c_write: error waiting for addr ACK (status=0x116)
i2c_read: error waiting for addr ACK (status=0x116)
i2c_write: error waiting for addr ACK (status=0x116)
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: <ethaddr> not set. Validating first E-fuse MAC
Could not get PHY for cpsw: addr 1
cpsw
Hit any key to stop autoboot: 2
and it will repet to output these information,we have no ID eeprom on our board,we don't know how to solve the iic write error.we see the the schematic about the idk on page 5,
the resistor R572 and R588 should be remove? or because of other problem?
our sdk version is ti-processor-sdk-linux-rt-am57xx-evm-03.03.00.04.