This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

JTAG connection error in DaVinci™ HD1080p EVM



Error 0x80000260/-1137

Fatal Error during: Execution, Initialization, OCS, 


It appears that the target is being held in reset.  This may be

due to Wait-In-Reset (WIR) configuration set by the EMU0=0

and EMU1=1 pin settings.  If this is the case, DISCONNECT

all CONNECTED devices including icepick and then select

RETRY to clear the WIR configuration.


If this is a multi-core system, the master CPU may not be

releasing the DSP/MCU from reset.  Please check your

configuration in CC_setup and/or your GEL file to ensure that

nothing is blocking the DSP/MCU from being released from reset



I/O Port = 510


Board Name: DAVINCI_HD_1080p_XDS510USB

Cpu Name: C64PLUS


Abort: Close Code Composer Studio.

Retry: Try to connect to the target again.

Cancel: Remain disconnected from the target

Diagnostic: Run diagnostic utility.

----------------------------------------------------------------------------------

-----------------------------------------------------------------------------

1,  software configuration:

my CCS version is 3.3.81.6.

I  already installed  setupCCSPlatinum_v30330.ZIP  and Patch_030330_XDS510USB_22sept2010.zip (downloaded from http://support.spectrumdigital.com/ccs33/)

Davinci™ HD1080p EVM CCS Config Files, Davinci™ HD1080p EVM DSP GEL File  and Davinci™ HD1080p EVM CCS Config Files

downloaded from http://support.spectrumdigital.com/boards/evmdm6467t/revc/.

 

 

2,  my hardware configruation are below:

JTAG Emulators  is   spectrum  digital XDS510 USB Plus.  

Switch SW3 configuration is  ALL(8 pin) is off.

S1,EMU0/1 Select Swtich configuration is EMU0 (H) and EMU1(H).

Dear Experts:

will you please tell me what 's the problem ?  thanks.