This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: The maximum bus access period of GPMC

Guru 10235 points

Part Number: AM5728

Hello, TI Experts,

 

Our customer sent us questions about GPMC of AM5728.

They want to know the maximum bus access period of GPMC as below condition.

  - Asynchronous Read/Write Access

  - GPMC_FCLK=266MHz (1clk=about 3.76ns)

 

Question1:

  Based on TRM(SPRUHZ6J) "15.4.4.8.4 Error Handling"

   - If GPMC_TIMEOUT_CONTROL.TIMEOUTSTARTVALUE is set to 0x1FF(=511),

     a time-out error occurs after over 511 GPMC_FCLK cycles past from the bus access-start.

     So, in this case, the effective maximum bus access period is 511xGPMC_FCLK (=about 1.92us).

Is this understanding correct?

 

Question2:

   For read access without wait pin monitoring,

   Based on TRM(SPRUHZ6J) "Figure 15-60. Wait Behavior During an Asynchronous Single Read Access"

   - The effective maximum bus access period is 31xGPMC_FCLK (=about 116.5ns),

       when GPMC_CONFIG5_i.RDCYCLETIME is set to 0x1F(=31).

   For Write access without wait pin monitoring, (TRM don't has the appropriate Figure)

   - The effective maximum bus access period is 31xGPMC_FCLK (=about 116.5ns),

       when GPMC_CONFIG5_i.WRCYCLETIME is set to 0x1F(=31).

            

   Is this understanding correct?

 

   If there are any way of extending bus access other than below, please tell us.

     - Configure RDCYCLETIME

     - Configure WRCYCLETIME

     - wait pin monitoring

 

Best regards,