Part Number: BEAGLEBK
Does the C function system("config-pin P9_41 pruin"); set ...
P9_41A in pruin / mode 5 to be read by __R31 bit 16 ... or ...
P9_41B in pruin / mode 6 to be read by __R31 bit 06 ???
>>> I want it to set the latter, i.e. P9_41B. instead of the former (because I need to use _PRU0 _R31 bit 16 to read P9_24).
-------- OR --------
Do I have to use the old device tree method for this?
Reference page 212 of Derek Molloy's Exploring Beaglebone Black book.