Hi
I am new to the processor SDK for Linux.
I have run the setup script, and I have a beaglebone running on minicom:
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyS0
Arago 2018.10 am335x-evm ttyS0
am335x-evm login: root
root@am335x-evm:~#
1. I booted the BBB several times and I always got a Debian Login screen ( username: debian, passwd: temppwd)
Then all of a sudden I got the Arago Boot screen above and I don't understand why
2. I try to crosscompile the Helloworld.c example:
$ ${INSTALLDir}/ti-processor-sdk-linux-am335x-evm-05.02.00.10/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-gcc helloworld.c -o helloworld
and I get:
helloworld.c:1:10: fatal error: stdio.h: No such file or directory
#include <stdio.h>
^~~~~~~~~
Do I need to install additional software after running the setup script ?
3) Is there somewhere a simple Helloworld example on how to run the entire toolchain, including developing and debugging on the host , making the exec available on the BBB and executing the code on the target ?
Thanks
Peter