Other Parts Discussed in Thread: OMAP-L132, OMAPL138
Do L138 secure part support basic secure boot from embedded eMMC flash memory?
Refer to "Using the OMAP-L132/L138 Bootloader", SPRAB41F document, section 6.5
"The MultiMedia Card/Secure Data (MMC/SD) boot mode is compliant with version 2.0 of the SD specification and version 4.2 of the enhanced MultiMedia Card (eMMC) specification."
I don't see any specification mentioned about the secure boot in eMMC (in document "TMS320C674x/OMAP-L1x Processor Security", SPRUGQ9).
I just need to configure the BOOT[5] pin to enable MMC boot and follow the procedure according to document SPRUGQ9 to enable the secure boot?