Dear Experts,
We have 4 AM3359 ICE development boards. The boards boot properly from SPI FLASH. But we cannot get the boards to boot from the SD card. We have followed the instruction in formatting the SD card and we copied various prebuilt MLO files and app files. We are using Tera Term set to 115200 BAUD. After power up we push the reset button and nothing come out.
Additionally we have a 4379 development board that we are using as a network TAP. This works properly from the SD card using the same format procedure. Obvioulsy the MLO and app files are different for the 4379 and the 3359. My point is that the SD card formatting is the same and works fine on the 4379.
We have completly erased the SPI FLASH on the 3359 and the boot jumpers are factory set. To erase the flash we used the SPI Flashing Tool (SPI_FLASH_WRITER_AM335X.out) through CCS to erase the SPI FLASH. It claims that it was successful.
We tried using a 32 and an 8 GByte SD cards that were formatted with FAT16 and FAT32. There was no difference.
We are stumped and need your help.
Thank you.
Drew