I burn the TI offered prebuilt image am65xx-hs-evm-linux-06.01.00.08.img to my new SD card. Then power on, I can't enter bootloader and nothing happened, why ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I burn the TI offered prebuilt image am65xx-hs-evm-linux-06.01.00.08.img to my new SD card. Then power on, I can't enter bootloader and nothing happened, why ?
Hi Victor,
Do you have HS-evm?
Also to get to boot loader you need to copy the following files to boot partition of your SD card:
tiboot3.bin, tispl.bin, u-boot.img, sysfw.itb.
Then you should be able to boot to u-boot prompt.
Regards,
Keerthy
Victor,
I suggest you try multiple SD cards, if you have not yet done so. Also, if you want to verify that the AM65x device is alive/running, I would set the board to UART boot mode and connect a terminal. If you see the "CCC..." xmodem download prompt, then you know that the SoC is running. You could even attempt to load the low-level boot image (tiboot3.bin) by doing an xmodem upload from your terminal program. Note that for a secure AM65x device, that image must be properly signed with the correct private evaluation key(s).
Regards, Daniel
Hi Daniel,
Yes, I have connected to UART console. It is just showed some value 0x8xxxxxx when I power on. I got the tiboot3.bin from TI web site. I got the new HS version board. How I sign the tiboot3.bin ? And what is the key ? Thank you.
Regards, Victor