Other Parts Discussed in Thread: MATHLIB
Hi TI Expert,
TMS320C6674 is used to realize my algorithm. The algorithm is mainly matrix operation. The calculation amount is about 1 trillion times plus operation. It is convert to C language (floating-point double) through MATLAB. The processing delay is 287ms by calculating the number of instruction cycle execution times on TMS320C6674, which is over expectation. I have several questions:
1. Could you give me any suggestion on reducing processing delay and increasing operation speed?
2. What is the difference between the processing speed of TMS320C6674 processor for fixed-point number and floating-point number? Now the algorithm is a floating-point number, is it necessary to convert the algorithm to a fixed-point number?
3. The current algorithm only has one core open. How do TMS320C6674 multi cores turn on automatically or need to be configured manually? Can you provide a demo or tutorial to open multi-core to improve the operation speed?
4. DDR3 cannot be read or written. How to configure it? Is there a tutorial or demo?
Thanks and Best regards,
Thomas