Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
[1] Can the OSPI interface be used to upload firmware and debug for the AM65x Industrial Development Kit (IDK)?
[2] Is it possible to write firmware and debug via the OSPI interface, using the stock CCSTUDIO-SITARA and/or XDS560v2 features/scripts, without editing anything, for an implementation like below:
Target Device: Sitara AM6526 (OSPI: Customer Confidential information...if needed, contact me offline)
Debugger: Spectrum Digital XDS560v2 or Blackhawk XDS560v2
IDE: CCS
[3] Can the Spectrum Digital XDS560v2 // Blackhawk XDS560v2 be connected to a 20pin ARM-JTAG connector?
(Is there a connector or adapter that comes with these products...?)
[4] Are there any tools you know of for testing the DDR3 memory? (Any tools that will help evaluate the DDR3 implementation)
For example, editing the timing parameters, and checking the DQ and DQS timing margins before a bit error is detected...
I really need an answer ASAP, and I am sorry to push, but even if it is a partial answer that would be appreciated.
Thanks!
Regards,
Darren
Is it possible to write firmware and debug via the QSPI interface, using the stock CCSTUDIO-SITARA and/or XDS560v2 features/scripts, without editing anything?
Target Device: Sitara AM6526 (OSPI: Customer Confidential information...if needed, contact me offline)
Debugger: Spectrum Digital XDS560v2 or Blackhawk XDS560v2
IDE: CCS