Hi Rafael,
I'm working with Pavel from the DSP board HW side.
I provided here some more information, with addition to what Pavel wrote, the following HW test were done as well:
1) CVDD measured to be 1.1V (although setting to 1.0V probably since the addition of 0.1V by the on board SmartReflex circuit).
2) CVDD1 was 1.0V
3) VCC1V8 measured to be 1.8V.
4) The CoreclockP and N was 100MHz the DSP Sysclock output was measured as expected and we could able to set as required.
5) The DDRclockP and N was measured and was as expected and we could able to set as required (started with 500MHz, 666MHz etc.
6) The DSP_RESETZ, DSP_PORZ, DSP_RESETFULLZ, DSP_LRESETNMIENZ signals were "H" level.
7) The power on sequence of CVDD, CVDD1, 1.8V, CoreClk and reset sequence was measured to be Ok.
8) All JTAG tests done by the XDS100 v3 were pass successfully.
The DSP and DDR3 supply pins and GND including the VDDT1, VDDT2, VDDR1, VDDR2 and all DDR3 supplies were connected as in the C6657 lite evm_sch_16-00132-02 schematics.
I can add that at the beginning the JTAG test were not pas but after adding serial resistors on the TMS,TDI,TDO, TCK and RCK signals the XDS100 target test was pass successfully.
If any additional test or information as schematics for review are required then we can provide it.
Can you suggest other tests and measurement in HW in order to verify proper work of the HW?
Is the JTAG target test successful pass means that the JTAG communication with the target DSP is reliable and can be trusted?
Thanks,
Moshe