Hi
I am trying to enable spi1 in am3358. But in am33xx.dtsi, i observed that spi1 and many things like i2c0, i2c2 all are disabled. But i2c0 is used internally in beaglebone black then why it is disabled in this file. can anyone help me to figure out why it is so given? I am using beaglebone black.
spi1: spi@481a0000 {
compatible = "ti,omap4-mcspi";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x481a0000 0x400>;
interrupts = <125>;
ti,spi-num-cs = <2>;
ti,hwmods = "spi1";
dmas = <&edma 42 0
&edma 43 0
&edma 44 0
&edma 45 0>;
dma-names = "tx0", "rx0", "tx1", "rx1";
status = "disabled";
};
i2c0: i2c@44e0b000 {
compatible = "ti,omap4-i2c";
#address-cells = <1>;
#size-cells = <0>;
ti,hwmods = "i2c1";
reg = <0x44e0b000 0x1000>;
interrupts = <70>;
status = "disabled";
};
Thanks & Regards
Sandeep Kumar