Other Parts Discussed in Thread: TPS65023
Hi,
We are using Processor P/N#TMS320C6746EZWT4, It is running at 456 MHz and its core supply Voltage is 1.3V. In our Design, Core Voltage is shorted with PLLx_VDDA, Whereas PLLx_VDDA voltage Min =1.14V, Typ=1.2 and Max 1.32V
P/N# TPS65023BRSBR is used to supply power for Processor. So the default tolerance of VDCDC1 = 2%. If I do worst case calculation 1.3V +2% = 1.326V (Approximately 6mV more than recommended).
Question
1) At What conditions, VDCDC1 of TPS65023BRSBR can go to +2% (1.326V)? I hope it will be very rare occurrence.
2) Even if VDCDC1 reaches 1.326V, will it impact Process PLLx_VDDA? It is just 6mV excess than the recommended Max voltage.
Regards,
Balaji A.