When Chromium is launched with:
chromium --no-sandbox
Sometimes it runs, other times it crashes. And there is a lot of error messages related to the GPU OpenGL interface. The Canvas GPU acceleration doesn't seem to work fine (probably because of these errors). The GPU load when running a real time chart using Canvas is only 5% (looks like GPU is not being used) and the load on the ARM processors is around 95%.
Is there a way I can run chromium with GPU acceleration? Like running chromium with s special flag configuration?
Attached are the GPU errors thrown when launching the browser: