Hi,
I am using TMS320C6678 at 1.25GHz, and I am using the power consumption excel sheet "6678_Power_Consumption_Summary_Rev3_4" for calculating current for different rails.
For voltage rail CVDD1, following currents are observed:
I_activity = 30 mA
I_baseline = 2.152 A
I_total = 2.182 A
(1) Is I(baseline) current all DC or does it have AC component too? Hardware design guideline (SPRABI2D) says that "The baseline power portion is associated with leakage, clock tree, and phase-locked loop (PLL) power." While leakage may be considered DC, I think clock tree and PLL power looks should have AC components. Kindly advise.
(2) What current component should be used decoupling analysis ? For my calculations, we see that if I_baseline doesn't contain AC component, then the decoupling capacitors requirement becomes very relaxed as the dynamic current is only 30mA (I_activity). However, if I_baseline also contains AC component, then how much current from I_baseline should we consider as AC for decoupling analysis?
(3) What current component should be used for DC drop analysis? Should I(total) be used or I(baseline) be used?
Thanks,
Binayak