In my application, the C6748 SPI1 is used as a slave, and another MCU ESP32 is used as a master. SPICLK=10MHz.
But the SPI commucation get errors sometimes, so I tried to find some examples using SPI as Slave.
Here I find the examples:
I read the above post and run the Master/Slave exmaple project using two C6748 EVM boards.
The SPI signals CLK\MOSI\MISO\CS and GND are connected using wires. I'm sure the the signals are well connected.
But running the examples, the Master and Slave will get error bit at the second transfer. I changed the CLK from 10MHz to 1MHz, but still has the problem.
Does anybody run the example and get everything right?
Or does anybody use C6748 as SPI slave and work normally?
Thank you.