Hi,
board:- 66ak2g12.
EVM:- EVMK2G.
PDK:- pdk_k2g_1_0_14.
tool:- CCS
we are testing ethernet interface in our project in that we are facing some issues,
1. For 1000 mbps speed ethernet interface is working in the EVM we can able to ping from Linux machine to our EVM.
2. For 100mbps speed ethernet interface is not working in the EVM we can't able to ping from Linux machine to our EVM. Link is not established.
observations:-
- If we configure the ethernet interface for 100mbps speed the Tx clock in the RGMII line is not changing from 125MHz to 25MHz.
- Even after setting the 100mbps SW is not Changing RGMII to 100mbps, but it is always fixed at 1G.
- Attached the EMAC Register Dump for your reference.
- EMAC_registers_dump.xlsx