Hi,
I am developing an Ethernet driver for PRU-ICSSG (SR 2.0) using dual mac firmware for AM6548 chip based on a proprietary RTOS.
I am using the SDK 7.01 based DUAL EMAC firmware from the below source:
Is there any speed performance benchmark for 1 Gbps and 100 Mbps for the emac Ethernet driver based on SDK 7.01 DUAL EMAC firmware?
It will be very helpful if you can provide me with some benchmark results so that I can compare with the performance of my Ethernet driver.
Best Regards,
Debarun