Hi,
In my configuration,I just config ptrLowPowerMode->lpAdcMode = LP_ADC_MODE_LOW_POWER; but I found in my 1843 device,the power up to 4.8w.When the wave start,the max cunrrent is 570mA,and what is more,in profile configuration ,I set tx_power_backoff_code = TX_POWER_BACKOFF_0DB,rx_gain_val = 52 | (1 << 6), /* VGA 52dB, Target Gain 34dB*/
What else can i do to reduce the power consumption?
Thanks!