This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7900: AFE7900

Part Number: AFE7900

 Hi,

I am interested to buy your product AFE7900, I have some questions to make sure if the item will be fit:

1. can I send Tx and RX RF in range 7.5GHz whiteout downconverter
as in your datasheet:
RF frequency range:
– TX: 5MHz - 7.4GHz
– RX/FB: 5MHz -7.4GHz


2. from AFE7900 datasheet the following info:

"Quad RF sampling 12-GSPS transmit DACs • Quad RF sampling 3-GSPS receive ADCs • Dual RF sampling 3-GSPS feedback (auxilliary RX) ADCs"

 is the maximum sampling at 3-GSPS?

is there full details of the datasheet?