Other Parts Discussed in Thread: AFE7952
Hello,
Are there any concerns or issues with developing on the AFE7920 & transitioning to an AFE7952 in the future?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Owen,
The AFE7952 is considered as a superset device to the AFE7920. The AFE7952 has more digital features to cover wider bandwidth, and can support higher RF frequency ranges. It is a pin-to-pin drop in. Therefore, if the customer starts to develop AFE7920, and wanted to transition to AFE7952 with more feature set support, this is completely OK.
-Kang