Other Parts Discussed in Thread: TX12
Q1:Does FB1TDD represent the enable GPIO control input for FB1?
Q2:Does TX12TDD represent the enable GPIO control input for TX12?
Q3:If TX12TDD is bound to GPIOB12, can the TX1 and TX2 RF channels be enabled or disabled by controlling the level of GPIOB12? Will both TX1 andTX2 be enabled or disabled together?
Q4:If GPIOB12 is set to 1, is TX1 enabled?