Other Parts Discussed in Thread: AFE7906, TSW14J57EVM,
Tool/software:
I am analyzing the specifications provided in the datasheet for the AFE7950 ADC converter, especially the SFDR values for different amplitudes of the input analog signal. As described, the ADC has an SFDR of:
- -71 dBFS for a -3 dBFS signal (frequency: 9610 MHz)
- -80 dBFS for a -13 dBFS signal (frequency: 9610 MHz)
From observing the graphs, it appears that the SFDR value improves as the amplitude of the input signal decreases, with the best SFDR value of -80 dBFS occurring for an input signal of -13 dBFS. I would like to confirm whether, for signals with amplitudes lower than -13 dBFS, the SFDR tends to become linear and remains close to the optimal value of -80 dBFS, or if there are other characteristics of the ADC's performance that we should consider for these lower amplitude signals.
The reason for this inquiry is the question of what is the smallest signal that the ADC converter can distinguish from noise, spurious, and harmonic distortions. I understand that if there is an SFDR of -80 dBFS, then a -75 dBFS signal would be distinguishable and converted by the ADC.
Thank you for your attention, and I look forward to your response.
Sincerely,
Luiz Gustavo.