Part Number: LM358
CAN SOMEONE EXPLAIN HOW THIS CIRCUIT WORKS AND WHAT EQUATIONS WHERE USED TO CALCULATE THE VALUES OF RESISTORS AND CAPACITORS.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM358
CAN SOMEONE EXPLAIN HOW THIS CIRCUIT WORKS AND WHAT EQUATIONS WHERE USED TO CALCULATE THE VALUES OF RESISTORS AND CAPACITORS.
John,
This is an inverting amplifier with a gain set very high. Basically 2.2M / ESR[C1] . ESR is the cap's resistance.
DC operating point IN1+ and OUT1 are set by a voltage divider. Jumping to conclusion 3.1V
3.1V at output lightly turns on voltage drops of T1 and LED1, so any signal could turn LED on brighter
At GSM frequencies the input cap C1 will actually appear to be inductive (past self resonance); so it is high impedance to GSM and a low impedance to 50/60Hz line
LM358 is not great at EMI rejection and the GSM creates a DC error that could raise the DC output which turns the LED brighter.
R3 limits the maximum LED current
Thank you for your answer . If you have time can you provide insight on the design equations used to calculate the values of the resistors and capacitors.
Voltage at pin 3 = V * R1 / (R1+R2)
Capacitor values are not critical. Like I said at GSM frequencies they do not act like capacitor's any more. At 50 or 60Hz the captative reactance will be low compared to resistors. Xc=1/6.28/F/C F=frequency, C = capacitance
T1 is a voltage follower , emitter output voltage = (base input voltage) - (base emitter drop voltage).
The base emitter voltage is a function of temperature and logarithm of collector current. Roughly 0.6V