Part Number: AFE7444EVM
Hi,
I noticed the SPI clock in the AFE7444EVM is around 30kHz.
can you tell me the process to increase it like 40 MHz. to its maximum speed.
With rggards,
Ganesh Singh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE7444EVM
Hi,
I noticed the SPI clock in the AFE7444EVM is around 30kHz.
can you tell me the process to increase it like 40 MHz. to its maximum speed.
With rggards,
Ganesh Singh
Hi Ganesh,
On the AFE7444EEVM, SPI clock speed is limited by the USB (FTDI) device protocol being used. It is not possible to increase the SCLK frequency to 40Mhz using EVM USB interface. Jumpers JP13 can be used to connect SPI bus to FMC (or tap out and be connected to external SPI driver).
Regards,
Vijay