Hi,
when we choose number of rx=2 or rx=1 in best velocity resolution demo visualizer is not working.Checked in ccs and program won't run after passing below config file and we are not getting any error message also. Please find the below configuration which we used.Is there any specific reason for this behaviour?
flushCfg
dfeDataOutputMode 1
channelCfg 2 1 0
adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 77 3888 7 18.24 0 0 27.412 1 64 6249 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 0
frameCfg 0 0 128 0 1000 1 0
guiMonitor -1 1 1 0 0 1 1
cfarCfg -1 0 0 8 4 4 0 640
cfarCfg -1 1 0 8 4 4 0 640
peakGrouping -1 1 1 1 1 63
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
sensorStart
Thanks,
Preetham