Hi team,
Could you give me comment on following customer question?
Q1. Is it correct understanding that the worst case accuracy is 5.5%RH as maximum, which consists of +/-3%RHACC,max and +/-2.5%RHLTD,max (=0.25%/yr*10yr)?
The RHLTD shows +/-0.25RH/yr as typical under typical conditions (at 30deg and 20% to 50% RH), but the customer is not sure what value is "maximum or worst case". Can 0.25%/yr be considered as worst case value?
Best regards,
Takeshi Sasaki