Other Parts Discussed in Thread: SYSCONFIG
Hello! I wanted to be able to see the Sync Out signal on AWR1843 Boost board while running the out of box demo code using the data visualizer GUI but it looks like R108 (the resistor between the AWR1843 and J6 pin 18) isn't populated for whatever reason (not entirely sure why it wouldn't be). All the same, I tried probing the signal at the pads and it looks like this functionality isn't enabled by default.
I downloaded the SysConfig program to generate the necessary code to be able to MUX this signal in and it gave me the following code to add this function (shown below):
I tried to find a place to implement this in and realized that the code I flashed in didn't have the source code, only the *.bin file (I used C:\ti\mmwave_sdk_03_05_00_04\firmware\radarss\xwr18xx_radarss_rprc.bin). In order to be able to add this line of code, I believe I'll need the source code. Is it possible to provide the source code so I can update it to add this line of code?
Any additional info that would be helpful would be greatly appreciated as well. Thanks for all your help!