Hello,
We are working on a project where were are using TMCS1100A3 current sensor to measure the motor current to control the motor. We want to run this motor continuously for extended hours. The motor runs for a few hours and stops. But there was current still flowing into the motor windings. On examining the current sensor signals, we found out that the sensor output is 0 V (should have some value when the current is still flowing through the windings), the supply voltage was still 5V and the reference voltage is 1.65 V reference (from a 3.3 V supply).. After we cycled the power to the circuit board, everything started to work properly again.
Can I get help in understanding why we are facing this problem? The current sensor first works properly for a few hours continuously which lets the motor to spin, and then at some point of time, it would stop working (give 0V at the output) despite having the 5 V supply and 1.65 V reference (from a 3.3 V supply). However, we cycle the power to the circuit and it starts working again. We want the current sensor to work continuously for extended hours without any interruption.
Please find below the circuit schematic we are using for the current sensor:
Please let me know if you need more information.
Thanking you in anticipation.
Best Regards,
Prasanth