Other Parts Discussed in Thread: TIDEP-0091,
In TIDEP-0091,IWR1443Boost is power-cycled by MSP432lLaunchpad。
We change frameCfg->numFrames to 0, and add demo_config1D_HWA(dataPathObj); demo_dataPathTrigger1D(dataPathObj); at the end of every measurement,
so the software continuous trigger the IWR1443Boost without MSP432Launchpad.
We also enable RUN_FULL_CAL.
We also designed a PTFE lens for iwr1443.
We use the profileCfg and frameCfg paremeters from sprcah9 Chirp Budget Calc_09_25_18.
It can not get the distance when the target is more than 20 meters using DEMO_CONFIG30.
It can get all the distance when using DEMO_CONFIG75, but the accuracy is very poor. The measuring error is about 1 meter at 50 meters range, 1.5meters at 60 range, more than 2 meters at 70 meters range
Please help us analyze it