こんにちは
DRV421搭載のmAセンサーを検討中です。
試作をした時は、0mA前後のエリアが非常に不安定です。
OPENLOOPをチェックすると、0の周りの応答はヒステリシスのようなもので、0の周りを安定してチェックできませんでした。
データシートのオフセットドリフトを確認するにはどうすればよいですか?
ありがとうございました
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
こんにちは
DRV421搭載のmAセンサーを検討中です。
試作をした時は、0mA前後のエリアが非常に不安定です。
OPENLOOPをチェックすると、0の周りの応答はヒステリシスのようなもので、0の周りを安定してチェックできませんでした。
データシートのオフセットドリフトを確認するにはどうすればよいですか?
ありがとうございました
Hello Kimihiko,
I used Google Translate and hopefully you can do the same or something similar. There are a few challenges with the DRV421 measuring low current. Please see this post which has links to other E2E post. As for the low values make sure your inductance of your compensation coil is high enough to keep the loop stable. See this Application Note. I assume that the closed loop works at higher current. A question on the open loop operation if the output is 0V then the device is already railed unless your 0V is measured in reference to the Vref pin.
To measure the drift I would calculate the magnetic gain seen at the DRV421 as the offset drift is done with field offset. Be aware that your magnetic core could get magnetized and be a contributor to the drift.
私はグーグル翻訳を使用しました、そしてうまくいけばあなたは同じか似たようなことをすることができます。低電流を測定するDRV421にはいくつかの課題があります。他のE2E投稿へのリンクがあるこの投稿を参照してください。低い値については、補償コイルのインダクタンスがループを安定させるのに十分高いことを確認してください。このアプリケーションノートを参照してください。閉ループはより高い電流で動作すると思います。出力が0Vの場合の開ループ動作に関する質問では、0VがVrefピンを基準にして測定されない限り、デバイスはすでにレール制御されています。
ドリフトを測定するために、オフセットドリフトがフィールドオフセットで行われるときにDRV421で見られる磁気ゲインを計算します。磁気コアが磁化され、ドリフトの原因となる可能性があることに注意してください。