Hello,
We are trying to develop a current transducer for residual current detection (RCD) and are looking into using the DRV241 in our design. The client needs to measure a range between -200 and +200 mA and a fault detection of 5 mA.
Reviewing the datasheet and the system parameter calculation available in the product page, we noted that the fluxgate sensor front-end offset would be the main issue for this application.
Is this offset specific for each IC or does it change over time? Would it be possible to calibrate the reading at the ADC during the assembly to reduce its effect?
Thank you.
Roberto