Thank you very much for your help.
Please let me know about LDC_COIL_EVM.
1. About sensor capacitors
Overview of the LDC Reference coils user's guide states that
Overview of the LDC Reference coils user's guide, it is stated that "Sensor capacitors are not included by default, so you will need to solder in appropriate sensor capacitors.
Is this also the case when connecting to the LDC0851_EVM with a 68PF capacitor mounted?
I actually connected the H coil of LDC_COIL_EVM to LDC0851EVM, but the sensing operation resulted in discontinuity.
2.Questions about the sensing operation
I conducted a sensing experiment by gradually increasing the distance between the sensor coil surface and a metal object, but the output from the LDC0851EVM does not turn ON at a specific detection distance.
For example, the output of LDC0851EVM turns ON when the end of the sensor coil is +16mm~+27mm.
For example, the output of LDC0851EVM turns ON when the sensor coil end is +16mm~+27mm, and the output of LDC0851EVM turns OFF when the sensor coil end is +27mm~+32mm.
The output of the LDC0851EVM turns ON for the sensor coil end +33mm~46mm.
The above is all I have to say.