Hi TI experts,
As there is a mistake for BOM, we got some 1443 based RADAR board with LP87524B power solution without LDO, i.e, 1.8V and 2.3V are powered to 1.0V and 1.8V power rails directly.
Although we kenw that is high risk for RADAR SoC, it woks "properly" now, just lost some detection range.
Can I change the voltage of LP 87524B using mmWavwSDK to meet the voltage requirements for 1443 without LDO.
There is an IIC interface connected between IWR1443 and LP87524B on our board, therefore, theoretically, there should be a way to change the output voltages of bulk2 and bulk3 of LP87524B, I wonder whether the SDK has support these operations and how to do it?
Thanks very much!
Best Regards.