Other Parts Discussed in Thread: TMP116
Hi,
Customer is pulling almost a full vacuum and are putting the board in a vacuum chamber and decreasing the pressure down to below 1 psia. Then after holding the vacuum for seconds or minutes, we pump air or gas back into the chamber.
Then later, they expose the board to high temp and high humidity conditions. While the chamber is ramping up temperature and humidity, the humidity sensor has a large offset (+ 15%RH). they have plenty of data from other boards with HDC2022 that does not have this +15%RH so we are trying to identify the root cause of the issue and have highlighted this vacuum event as one potential area of investigation.
Now the datasheet mentions that exposing the device beyond the recommended 20%-80% RH can cause shift in sensor readings. Can you please provide some feedback if you have seen something similar before? Are the devices damaged? are such tests recommended? How long is the expected recovery time? etc...
Thank you for your support!
Aivy