Other Parts Discussed in Thread: AWR1843
I am using the AWR1843 Boost to capture XYZ data from a thick dielectric object. The interface is air and the Range boxes are set up based on air dielectric and velocity = C). The dielectric constant of the object is unknown. Would the X, Y, and Z from the range and scatter plots be accurate since they would be based on the air dielectric? There is refraction as expected but I am unsure if using the X, and Y dimensions from the plots to calculate the angle would be correct. Is this already accounted for in the TI's analyses?