We are trying to use LDC1612 for distance measurement. Below are the settings
-- RCOUNT 0xFFFF
-- FREF Divider = 1
-- FREF = 40MHZ
-- FIN: Looking at the scope we are getting close to 550kHz
With these setting per some application notes we should get less than one HZ of resolution. But we seem to have code variation (repeatability) of +/-200 codes. Any way to get this more stable?
-- We are using both sensors: Will using only one sensor make the performance more stable?
-- If there is inherent variation in LC frequency, what might be the root cause? Power supply variations? Or any other factors
-- If we reduce the parallel capacitance (currently at 390pF) it will increase the frequency, will it improve stability?
-- Any other ideas?