Hi team,
My customer need assistance:
Question Details:
Set register ZC_CONFIG:0XB1
Schematic as follows, test point: connector P3-pin1, IC U3-pin1
- Waveform as follows:(yellow--P3-pin1,green--U3-pin1)
We can see within the first cycle ZC output OUT3 action normal, low-->high when signal higher than threshold value and high-->low when lower than this value; but the logic is not correct in the following cycles, please help to check why?
- Almost the same input signal, the OUT3 action is different:
In the follow pictures, original signal--yellow, OUT3 output--green,
We can see in the second picture OUT3 not changed when the signal became higher whthin the first cycle while different action in the first picture,
Need to check why this happened?
Kindly check and help. Thanks.