This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to know if there is a way that the IWR6843 could identify itself as either being ES1.0 or ES2.0. Can you query one or both of the cores for this information and if so, how? Or is there any other tell tale sign?
Hi,
Please refer to the markings on the package itself to determine if the device is ES1.0 or ES2.0 as explained in the image below.
Best Regards,
Josh
Josh Dye Thank you the reply -- but is there any programmatic way in the firmware, i.e. something like a version command?
Hi,
The mmw demo provides the "version" command which you can run on the CLI to get this information.
Best Regards,
Josh