Other Parts Discussed in Thread: TIDEP-01006, IWR6843ISK, IWR6843ISK-ODS,
Hi Team, seeking some inputs
1. what the maximum range for people detection and whether this changes based on whether I choose the AOP vs non AOP vs ISK vs EVM
2. I noticed that for most of the demos, even those related to automotive radar applications, the mmWave chip is stationary. However, with [TIDEP-01006] the demo board is mounted to a moving robot. The GUI of captured data shows the surroundings as fixed and the robot/sensor as moving. Is a MEMs accelerometer required to calibrate the sensor for applications like this where it will be mounted to a moving object? Or no extra hardware is needed even for applications when the sensor is mobile?
Thank you in advance.
-Mark