Hi,
I am using txOutPower to decrease out power of Tx antennas, here is the related configuration:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using txOutPower to decrease out power of Tx antennas, here is the related configuration:
Hello.
The TX output power back-off code is 1) not in dB and 2) in decimal notation but from a converted hex number. It is a 24 bit value, with every 8 bits representing the TX backoff for each transmitter. For example, for a 10 dB back off for all 3 transmitters, the hex number would be 0A0A0A, which then converted to decimal is 657930. You can do the same with 30 dB as well. As a result, putting 30 as the parameter value in profileCfg is very close to 0 dB backoff, which is why you are still getting the detected points.
Hope this helps,
Santosh
Because I only use one Tx, so I think 30 is OK.
Set the back-off code to 1973790, which is 0x1E1E1E. The output is the same as the above figure.
So, why there are still some detected points? Thanks.
Hello Jun.
The power on that scale is relative so you won't see a major drop off even with a reduction in transmit power. Also, why are you not trying to detect points?
Sincerely,
Santosh
OK. I just want to confirm that the transmit power is actually decreased.
Thanks.